CircularImprintBuilder Class¶
-
class
NXOpen.CAE.
CircularImprintBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Circular Imprint
To create a new instance of this class, use
NXOpen.CAE.AbstractionManager.CreateCircularImprintBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AbsoluteDiaAroundEdge | Returns an absolute dia around edge |
AbsoluteDiaAroundPoint | Returns an absolute dia around point |
AroundEdgeDiaOption | Returns or sets an around edge dia option |
DiaScaleFactor | Returns or sets the dia scale factor |
EdgeSelection | Returns the selected edge/point object(s) |
SurfaceSelection | Returns the selected surface object(s) |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CircularImprintBuilderAroundEdgeDiaType Enumeration | Around Edge Diameter Option |
Property Detail¶
AbsoluteDiaAroundEdge¶
-
CircularImprintBuilder.
AbsoluteDiaAroundEdge
¶ Returns an absolute dia around edge
-------------------------------------
Getter Method
Signature
AbsoluteDiaAroundEdge
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
AbsoluteDiaAroundPoint¶
-
CircularImprintBuilder.
AbsoluteDiaAroundPoint
¶ Returns an absolute dia around point
-------------------------------------
Getter Method
Signature
AbsoluteDiaAroundPoint
Returns: Return type: NXOpen.Expression
New in version NX7.5.0.
License requirements: None.
AroundEdgeDiaOption¶
-
CircularImprintBuilder.
AroundEdgeDiaOption
¶ Returns or sets an around edge dia option
-------------------------------------
Getter Method
Signature
AroundEdgeDiaOption
Returns: Return type: NXOpen.CAE.CircularImprintBuilderAroundEdgeDiaType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AroundEdgeDiaOption
Parameters: methodOption ( NXOpen.CAE.CircularImprintBuilderAroundEdgeDiaType
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
DiaScaleFactor¶
-
CircularImprintBuilder.
DiaScaleFactor
¶ Returns or sets the dia scale factor
-------------------------------------
Getter Method
Signature
DiaScaleFactor
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiaScaleFactor
Parameters: dia (float) – New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EdgeSelection¶
-
CircularImprintBuilder.
EdgeSelection
¶ Returns the selected edge/point object(s)
-------------------------------------
Getter Method
Signature
EdgeSelection
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX7.5.0.
License requirements: None.
SurfaceSelection¶
-
CircularImprintBuilder.
SurfaceSelection
¶ Returns the selected surface object(s)
-------------------------------------
Getter Method
Signature
SurfaceSelection
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
CircularImprintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.