CfdLocalResolutionConstraintBuilderSizing Enumeration

NXOpen.CAE.CfdLocalResolutionConstraintBuilder.Sizing is an alias for NXOpen.CAE.CfdLocalResolutionConstraintBuilderSizing

class NXOpen.CAE.CfdLocalResolutionConstraintBuilderSizing

Bases: object

The sizing option.

Enum Members

Enum Member Enum Member Description
RelativeRefinement
RelativeCoarsening
Absolute
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.