CfdLocalResolutionConstraintBuilderLocalSubdivisions Enumeration

NXOpen.CAE.CfdLocalResolutionConstraintBuilder.LocalSubdivisions is an alias for NXOpen.CAE.CfdLocalResolutionConstraintBuilderLocalSubdivisions

class NXOpen.CAE.CfdLocalResolutionConstraintBuilderLocalSubdivisions

Bases: object

The local subdivision.

Enum Members

Enum Member Enum Member Description
Zero
One
Two
Three
Four
Five
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.