CfdContactPreventionConstraintBuilderPriority Enumeration

NXOpen.CAE.CfdContactPreventionConstraintBuilder.Priority is an alias for NXOpen.CAE.CfdContactPreventionConstraintBuilderPriority

class NXOpen.CAE.CfdContactPreventionConstraintBuilderPriority

Bases: object

The priority level.

Enum Members

Enum Member Enum Member Description
Low
Medium
High
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.