CfdAutoRefinementConstraintBuilderLocalSubdivisions Enumeration¶
NXOpen.CAE.CfdAutoRefinementConstraintBuilder.LocalSubdivisions is an alias for NXOpen.CAE.CfdAutoRefinementConstraintBuilderLocalSubdivisions
-
class
NXOpen.CAE.
CfdAutoRefinementConstraintBuilderLocalSubdivisions
¶ Bases:
object
The maximum local subdivision
Enum Members
Enum Member Enum Member Description Zero No local subdivision One One level of subdivision Two Two levels of subdivision Three Three levels of subdivision Four Four levels of subdivision Five Five levels of subdivision -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-