CaeSetObjectSubType Enumeration¶
-
class
NXOpen.CAE.
CaeSetObjectSubType
¶ Bases:
object
Used to specify the sub type of selected objects e.g face of an element, edge of an element ..etc Enum Members
Enum Member Enum Member Description NotSet sub type is the same as the type of the object ElementFace sub type is element face ElementEdge sub type is element edge Part sub type is part, used for Gravity Loads SelRecipe sub type is selection recipe -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-