CaeRegionCollection Class¶
-
class
NXOpen.CAE.
CaeRegionCollection
¶ Bases:
object
Provides methods for managing
CAE.CaeRegion
in a sim partTo obtain an instance of this class, refer to
NXOpen.CAE.SimSimulation
New in version NX7.0.0.
Methods¶
Method | Description |
---|---|
Copy | Copies a CAE.CaeRegion |
CreateCaeRegion | Creates a CAE.CaeRegion |
FindObject | Finds the CAE.CaeRegion with the given identifier as recorded in a journal. |
Method Detail¶
Copy¶
-
CaeRegionCollection.
Copy
¶ Copies a
CAE.CaeRegion
Signature
Copy(tSourceRegion)
Parameters: tSourceRegion ( NXOpen.CAE.CaeRegion
) – source region to be copiedReturns: newly created region Return type: NXOpen.CAE.CaeRegion
New in version NX7.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateCaeRegion¶
-
CaeRegionCollection.
CreateCaeRegion
¶ Creates a
CAE.CaeRegion
Signature
CreateCaeRegion(descriptorName, name, label)
Parameters: - descriptorName (str) – Name of the region descriptor
- name (str) – Name of the region
- label (int) – Label of the region, input 0 to get next available label
Returns: Region object created
Return type: New in version NX7.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
CaeRegionCollection.
FindObject
¶ Finds the
CAE.CaeRegion
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: Region found Return type: NXOpen.CAE.CaeRegion
New in version NX7.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)