CaePartFieldApplicationType Enumeration¶
NXOpen.CAE.CaePart.FieldApplicationType is an alias for NXOpen.CAE.CaePartFieldApplicationType
-
class
NXOpen.CAE.
CaePartFieldApplicationType
¶ Bases:
object
Enumeration which is used to specify the type of field application to retrieve in the GetApplication method. This enumeration can be extended in the future when new field applications are created.
Enum Members
Enum Member Enum Member Description SignalProcessing Application which allows to specify additional attributes (e.g. acoustical weighting) on a field -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-