CaeGroupCollectionEntityType Enumeration

NXOpen.CAE.CaeGroupCollection.EntityType is an alias for NXOpen.CAE.CaeGroupCollectionEntityType

class NXOpen.CAE.CaeGroupCollectionEntityType

Bases: object

Entity type

Enum Members

Enum Member Enum Member Description
Node
Element
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.