CAEWeldConnectionBuilderMeshDensityTypeEnum Enumeration¶
NXOpen.CAE.CAEWeldConnectionBuilder.MeshDensityTypeEnum is an alias for NXOpen.CAE.CAEWeldConnectionBuilderMeshDensityTypeEnum
-
class
NXOpen.CAE.
CAEWeldConnectionBuilderMeshDensityTypeEnum
¶ Bases:
object
the mesh density type enum
Enum Members
Enum Member Enum Member Description Size Size of the each element on the hard object Number Number of elements on the hard object -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-