CAEConnectionBuilderPointToEdgeConnectionMethodTypeEnum Enumeration¶
NXOpen.CAE.CAEConnectionBuilder.PointToEdgeConnectionMethodTypeEnum is an alias for NXOpen.CAE.CAEConnectionBuilderPointToEdgeConnectionMethodTypeEnum
-
class
NXOpen.CAE.
CAEConnectionBuilderPointToEdgeConnectionMethodTypeEnum
¶ Bases:
object
the method of point to edge connection to be created
Enum Members
Enum Member Enum Member Description PointToEdge Create connection between point on source and target edges. ArcToCenter Create connection between arc or circular edge and its center. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-