CAEConnectionBuilderMethodTypeEnum Enumeration¶
NXOpen.CAE.CAEConnectionBuilder.MethodTypeEnum is an alias for NXOpen.CAE.CAEConnectionBuilderMethodTypeEnum
-
class
NXOpen.CAE.
CAEConnectionBuilderMethodTypeEnum
¶ Bases:
object
the method of connection to be created
Enum Members
Enum Member Enum Member Description Proximity Based on proximity OrderOfSelection In order of selection MeanVector Based on Mean Vector SortXcoord Based on sorted X coordinates SortYcoord Based on sorted Y coordinates SortZcoord Based on sorted Z coordinates Rbe3ToEdgeNodes Create spider element using projected node and edge nodes Rbe3ToFaceNodes Create spider element using projected node and adjacent face nodes -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-