CAEConnectionBuilderEdgeToEdgeConnectionMethodTypeEnum Enumeration¶
NXOpen.CAE.CAEConnectionBuilder.EdgeToEdgeConnectionMethodTypeEnum is an alias for NXOpen.CAE.CAEConnectionBuilderEdgeToEdgeConnectionMethodTypeEnum
-
class
NXOpen.CAE.
CAEConnectionBuilderEdgeToEdgeConnectionMethodTypeEnum
¶ Bases:
object
the method of edge to edge connection to be created
Enum Members
Enum Member Enum Member Description NodeToNode Create elements between nodes on source and target edges. Rbe2Rbe3ToElementEdge Create RBE2 between source node and projected node, and RBE3 between projected node and target edge nodes. Rbe2Rbe3ToElementFace Create RBE2 bewteen source node and projected node, and RBE3 between projected node and target face nodes. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-