CAEConnectionBuilderConnectionTypeEnum Enumeration¶
NXOpen.CAE.CAEConnectionBuilder.ConnectionTypeEnum is an alias for NXOpen.CAE.CAEConnectionBuilderConnectionTypeEnum
-
class
NXOpen.CAE.
CAEConnectionBuilderConnectionTypeEnum
¶ Bases:
object
the type of connection to be created
Enum Members
Enum Member Enum Member Description NodeToNode between nodes ElemedgeToElemface between element edges and faces PointToPoint between points PointToEdge between points and edges PointToFace between points and faces EdgeToEdge between edges EdgeToFace between edges and faces -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-