BeamSectionOrientationOptionsMethod Enumeration

NXOpen.CAE.BeamSectionOrientationOptions.Method is an alias for NXOpen.CAE.BeamSectionOrientationOptionsMethod

class NXOpen.CAE.BeamSectionOrientationOptionsMethod

Bases: object

Represents the orientation definition method

Enum Members

Enum Member Enum Member Description
ByVector
ByNode
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.