BcLabelManagerBuilderRenumberType Enumeration¶
NXOpen.CAE.BcLabelManagerBuilder.RenumberType is an alias for NXOpen.CAE.BcLabelManagerBuilderRenumberType
-
class
NXOpen.CAE.
BcLabelManagerBuilderRenumberType
¶ Bases:
object
Renumber Method
Enum Members
Enum Member Enum Member Description Renumber All the selected BC ID will be renumbered strarting from this number Offset All the selected BC ID will offset by this number -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-