BaseIterationIterationValueType Enumeration¶
NXOpen.CAE.BaseIteration.IterationValueType is an alias for NXOpen.CAE.BaseIterationIterationValueType
-
class
NXOpen.CAE.
BaseIterationIterationValueType
¶ Bases:
object
The type of value that is stored in a iteration object
Enum Members
Enum Member Enum Member Description Unknown Value has an Unknown type Time Value represents a Time Frequency Value represents a Frequency LoadFactor Value represents a LoadFactor Eigenvalue Value represents a Eigenvalue Harmonic Value represents a Harmonic RotationSpeed Value represents a RotationSpeed DesignCycle Value represents a DesignCycle Acoustic Value represents a Acoustic Mode -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-