BaseIterationIterationType Enumeration¶
NXOpen.CAE.BaseIteration.IterationType is an alias for NXOpen.CAE.BaseIterationIterationType
-
class
NXOpen.CAE.
BaseIterationIterationType
¶ Bases:
object
The Analysis type of a iteration object
Enum Members
Enum Member Enum Member Description Unknown Iteration has an Unknown type Static Static Analysis Iteration Mode Modal Analysis Iteration ConstraintMode Constraint Modal Analysis Iteration Transient Transient Analysis Iteration Buckling Buckling Analysis Iteration Nonlinear NonLinear Analysis Iteration FrequencyResponse Frequency Response Analysis Iteration -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-