AxiSymmetricParametersGetResult Enumeration

NXOpen.CAE.AxiSymmetricParameters.GetResult is an alias for NXOpen.CAE.AxiSymmetricParametersGetResult

class NXOpen.CAE.AxiSymmetricParametersGetResult

Bases: object

Axi Symmetric result type

Enum Members

Enum Member Enum Member Description
OnOriginalModel
RevolvedModel
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.