AxiSymmetricParametersAxisOfRotation Enumeration¶
NXOpen.CAE.AxiSymmetricParameters.AxisOfRotation is an alias for NXOpen.CAE.AxiSymmetricParametersAxisOfRotation
-
class
NXOpen.CAE.
AxiSymmetricParametersAxisOfRotation
¶ Bases:
object
Axis of rotation
Enum Members
Enum Member Enum Member Description XAxis YAxis ZAxis -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-