AutoPairsBuilder Class¶
-
class
NXOpen.CAE.
AutoPairsBuilder
¶ Bases:
NXOpen.Builder
Builds a
NXOpen.CAE.AutoPairs
object which represets a recipe for generating face pairs from a selected set of faces or solids in the model whose distance is less than a specified tolerance.To create a new instance of this class, use
NXOpen.CAE.SimSimulation.CreateAutoPairsBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
GeometrySelection | Returns the geometry selection |
PropertyTable | Returns the AutoPair’s property table |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
PreviewButton | Preview the list of face-pairs |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
GeometrySelection¶
-
AutoPairsBuilder.
GeometrySelection
¶ Returns the geometry selection
-------------------------------------
Getter Method
Signature
GeometrySelection
Returns: Return type: NXOpen.CAE.SelectCAEFaceList
New in version NX5.0.0.
License requirements: None.
PropertyTable¶
-
AutoPairsBuilder.
PropertyTable
¶ Returns the AutoPair’s property table
-------------------------------------
Getter Method
Signature
PropertyTable
Returns: Return type: NXOpen.CAE.PropertyTable
New in version NX5.0.0.
License requirements: None.
Method Detail¶
PreviewButton¶
-
AutoPairsBuilder.
PreviewButton
¶ Preview the list of face-pairs
Signature
PreviewButton()
New in version NX5.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
AutoPairsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.