AutoHealGeometryBuilder Class¶
-
class
NXOpen.CAE.
AutoHealGeometryBuilder
¶ Bases:
NXOpen.Builder
Builder for creating Auto Heal Geometry
To create a new instance of this class, use
NXOpen.CAE.AbstractionManager.CreateAutoHealGeometryBuilder()
Default values.
Property Value CurvatureAbstractionSetting 0 MergeEdgeSetting 0 Tolerance.Value 0 (millimeters part), 0 (inches part) VertexAngle.Value 15 New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
CurvatureAbstractionSetting | Returns or sets the curvature abstraction option |
MergeEdgeSetting | Returns or sets the merge edge option |
Selection | Returns the selection |
Tag | Returns the Tag for this object. |
Tolerance | Returns the minimum element length tolerance |
VertexAngle | Returns the vertex angle criterion used in merging edges |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
SmallFeatureAutoSize | The autogenerate minimum element length button |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CurvatureAbstractionSetting¶
-
AutoHealGeometryBuilder.
CurvatureAbstractionSetting
¶ Returns or sets the curvature abstraction option
-------------------------------------
Getter Method
Signature
CurvatureAbstractionSetting
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurvatureAbstractionSetting
Parameters: curvatureAbstractionSetting (bool) – New in version NX11.0.0.
License requirements: None.
MergeEdgeSetting¶
-
AutoHealGeometryBuilder.
MergeEdgeSetting
¶ Returns or sets the merge edge option
-------------------------------------
Getter Method
Signature
MergeEdgeSetting
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MergeEdgeSetting
Parameters: mergeEdgeSetting (bool) – New in version NX11.0.0.
License requirements: None.
Selection¶
-
AutoHealGeometryBuilder.
Selection
¶ Returns the selection
-------------------------------------
Getter Method
Signature
Selection
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
Tolerance¶
-
AutoHealGeometryBuilder.
Tolerance
¶ Returns the minimum element length tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
VertexAngle¶
-
AutoHealGeometryBuilder.
VertexAngle
¶ Returns the vertex angle criterion used in merging edges
-------------------------------------
Getter Method
Signature
VertexAngle
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
SmallFeatureAutoSize¶
-
AutoHealGeometryBuilder.
SmallFeatureAutoSize
¶ The autogenerate minimum element length button
Signature
SmallFeatureAutoSize()
New in version NX11.0.0.
License requirements: None.
Validate¶
-
AutoHealGeometryBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.