AutoBCBuilder Class¶
-
class
NXOpen.CAE.
AutoBCBuilder
¶ Bases:
NXOpen.Builder
Builds one or more
NXOpen.CAE.SimSimulationObject
object(s).These simulation objects use two target face sets like the Surf to Surf Contact
To create a new instance of this class, use
NXOpen.CAE.SimSimulation.CreateAutoBcBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Autopairs | Returns or sets the AutoBC’s NXOpen.CAE.AutoPairs |
BcBaseName | Returns or sets the base name of NXOpen.CAE.SimBC objects created |
DestinationFolder | Returns or sets the destination folder of NXOpen.CAE.SimBC object |
Label | Returns or sets the initial label of NXOpen.CAE.CaeRegion and NXOpen.CAE.SimBC objects |
PropertyTable | Returns the AutoBC’s NXOpen.CAE.PropertyTable |
Recipe | Returns the AutoBC’s NXOpen.CAE.SimAutoBcRecipe |
RetainRecipeFlag | Returns or sets the retain recipe flag, which signifies whether or not the recipe will be retained after the generation of the BCs |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Autopairs¶
-
AutoBCBuilder.
Autopairs
¶ Returns or sets the AutoBC’s
NXOpen.CAE.AutoPairs
-------------------------------------
Getter Method
Signature
Autopairs
Returns: auto pairs object Return type: NXOpen.CAE.AutoPairs
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Autopairs
Parameters: recipe ( NXOpen.CAE.AutoPairs
) – auto pairs objectNew in version NX5.0.0.
License requirements: None.
BcBaseName¶
-
AutoBCBuilder.
BcBaseName
¶ Returns or sets the base name of
NXOpen.CAE.SimBC
objects created-------------------------------------
Getter Method
Signature
BcBaseName
Returns: the base name Return type: str New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BcBaseName
Parameters: name (str) – the base name, if None or blank, a base name will be generated New in version NX8.0.0.
License requirements: None.
DestinationFolder¶
-
AutoBCBuilder.
DestinationFolder
¶ Returns or sets the destination folder of
NXOpen.CAE.SimBC
object-------------------------------------
Getter Method
Signature
DestinationFolder
Returns: destination folder Return type: NXOpen.CAE.SimLbcFolder
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DestinationFolder
Parameters: folder ( NXOpen.CAE.SimLbcFolder
) – destination folderNew in version NX9.0.0.
License requirements: None.
Label¶
-
AutoBCBuilder.
Label
¶ Returns or sets the initial label of
NXOpen.CAE.CaeRegion
andNXOpen.CAE.SimBC
objects-------------------------------------
Getter Method
Signature
Label
Returns: the initial label Return type: int New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Label
Parameters: label (int) – the initial label, if <=0 unique labels will be generated for you New in version NX8.0.0.
License requirements: None.
PropertyTable¶
-
AutoBCBuilder.
PropertyTable
¶ Returns the AutoBC’s
NXOpen.CAE.PropertyTable
-------------------------------------
Getter Method
Signature
PropertyTable
Returns: Return type: NXOpen.CAE.PropertyTable
New in version NX5.0.0.
License requirements: None.
Recipe¶
-
AutoBCBuilder.
Recipe
¶ Returns the AutoBC’s
NXOpen.CAE.SimAutoBcRecipe
-------------------------------------
Getter Method
Signature
Recipe
Returns: auto BC recipe Return type: NXOpen.CAE.SimAutoBcRecipe
New in version NX5.0.0.
License requirements: None.
RetainRecipeFlag¶
-
AutoBCBuilder.
RetainRecipeFlag
¶ Returns or sets the retain recipe flag, which signifies whether or not the recipe will be retained after the generation of the BCs
-------------------------------------
Getter Method
Signature
RetainRecipeFlag
Returns: flag for retaining recipe or not Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RetainRecipeFlag
Parameters: retainRecipe (bool) – flag for retaining recipe or not New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AutoBCBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.