AtvSetCollection Class¶
-
class
NXOpen.CAE.
AtvSetCollection
¶ Bases:
object
This class is a collection of
NXOpen.CAE.AtvSet
.To obtain an instance of this class, refer to
NXOpen.CAE.CaePart
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateBuilder | Creates an atvset builder. |
Delete | Delete an ATV Set |
Find | Finds a ATV Set with a specified name. |
Method Detail¶
CreateBuilder¶
-
AtvSetCollection.
CreateBuilder
¶ Creates an atvset builder.
Signature
CreateBuilder(pAtvSet)
Parameters: pAtvSet ( NXOpen.CAE.AtvSet
) – the Atv Set to edit, nullptr if being createdReturns: the builder Return type: NXOpen.CAE.AtvSetBuilder
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
Delete¶
-
AtvSetCollection.
Delete
¶ Delete an ATV Set
Signature
Delete(atvSetTag)
Parameters: atvSetTag ( NXOpen.CAE.AtvSet
) – The ATV Set to be deletedNew in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Find¶
-
AtvSetCollection.
Find
¶ Finds a ATV Set with a specified name.
Signature
Find(name)
Parameters: name (str) – name of the ATV Set Returns: Return type: NXOpen.CAE.AtvSet
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)