AttachElementsBuilder Class¶
-
class
NXOpen.CAE.
AttachElementsBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.AttachElementsBuilder
To create a new instance of this class, use
NXOpen.CAE.NodeElementManager.CreateAttachElementsBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
AttachType | Returns or sets an attach option |
EdgeCurve | Returns the curve |
ElementEdges | Returns the element edges |
MeshSelection | Returns the selected mesh |
PointEnd | Returns or sets an end point |
PointStart | Returns or sets a start point |
SplitLineType | Returns or sets a split line option |
SplitSize | Returns the split size |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AttachElementsBuilderAttachOption Enumeration | attach types |
AttachElementsBuilderSplitLineOption Enumeration | split line types |
Property Detail¶
AttachType¶
-
AttachElementsBuilder.
AttachType
¶ Returns or sets an attach option
-------------------------------------
Getter Method
Signature
AttachType
Returns: Return type: NXOpen.CAE.AttachElementsBuilderAttachOption
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttachType
Parameters: attachmentType ( NXOpen.CAE.AttachElementsBuilderAttachOption
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EdgeCurve¶
-
AttachElementsBuilder.
EdgeCurve
¶ Returns the curve
-------------------------------------
Getter Method
Signature
EdgeCurve
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX11.0.0.
License requirements: None.
ElementEdges¶
-
AttachElementsBuilder.
ElementEdges
¶ Returns the element edges
-------------------------------------
Getter Method
Signature
ElementEdges
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX11.0.0.
License requirements: None.
MeshSelection¶
-
AttachElementsBuilder.
MeshSelection
¶ Returns the selected mesh
-------------------------------------
Getter Method
Signature
MeshSelection
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX11.0.0.
License requirements: None.
PointEnd¶
-
AttachElementsBuilder.
PointEnd
¶ Returns or sets an end point
-------------------------------------
Getter Method
Signature
PointEnd
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointEnd
Parameters: endPoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PointStart¶
-
AttachElementsBuilder.
PointStart
¶ Returns or sets a start point
-------------------------------------
Getter Method
Signature
PointStart
Returns: Return type: NXOpen.Point
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointStart
Parameters: startPoint ( NXOpen.Point
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SplitLineType¶
-
AttachElementsBuilder.
SplitLineType
¶ Returns or sets a split line option
-------------------------------------
Getter Method
Signature
SplitLineType
Returns: Return type: NXOpen.CAE.AttachElementsBuilderSplitLineOption
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SplitLineType
Parameters: lineType ( NXOpen.CAE.AttachElementsBuilderSplitLineOption
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SplitSize¶
-
AttachElementsBuilder.
SplitSize
¶ Returns the split size
-------------------------------------
Getter Method
Signature
SplitSize
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
AttachElementsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.