AssignNodalCSBuilderGeometryOption Enumeration

NXOpen.CAE.AssignNodalCSBuilder.GeometryOption is an alias for NXOpen.CAE.AssignNodalCSBuilderGeometryOption

class NXOpen.CAE.AssignNodalCSBuilderGeometryOption

Bases: object

the geometry options

Enum Members

Enum Member Enum Member Description
InteriorNodesOnly interior nodes only
BoundaryNodesOnly boundary nodes only
InteriorandBoundaryNodes interior and boundary
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.