AssignNodalCSBuilderCs Enumeration

NXOpen.CAE.AssignNodalCSBuilder.Cs is an alias for NXOpen.CAE.AssignNodalCSBuilderCs

class NXOpen.CAE.AssignNodalCSBuilderCs

Bases: object

Assign CS options

Enum Members

Enum Member Enum Member Description
DisplacementCS displacement only
ReferenceCS reference only
Both reference and displacement
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.