AfuMathOperationTimeToSrsResponseType Enumeration¶
NXOpen.CAE.AfuMathOperation.TimeToSrsResponseType is an alias for NXOpen.CAE.AfuMathOperationTimeToSrsResponseType
-
class
NXOpen.CAE.
AfuMathOperationTimeToSrsResponseType
¶ Bases:
object
Defines the response type paramater for TIME to SRS
Enum Members
Enum Member Enum Member Description PositiveMax Positive Maximum NegativeMax Negative Maximum AbsoluteMax Absolute Maximum -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-