AfuMathOperationTimeToSrsAxisType Enumeration¶
NXOpen.CAE.AfuMathOperation.TimeToSrsAxisType is an alias for NXOpen.CAE.AfuMathOperationTimeToSrsAxisType
-
class
NXOpen.CAE.
AfuMathOperationTimeToSrsAxisType
¶ Bases:
object
Defines the frequency axis type for TIME to SRS
Enum Members
Enum Member Enum Member Description Linear Linear Log Log Octave Octave OneThirdOctave 1/3 Octave Decade Points per Standard Decade -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-