AfuMathOperationSrsToTimeStrategy Enumeration¶
NXOpen.CAE.AfuMathOperation.SrsToTimeStrategy is an alias for NXOpen.CAE.AfuMathOperationSrsToTimeStrategy
-
class
NXOpen.CAE.
AfuMathOperationSrsToTimeStrategy
¶ Bases:
object
Defines the conversion strategy for SRS to TIME when using the Wavelet method
Enum Members
Enum Member Enum Member Description Random Random conversion strategy ReverseSineSweep Reverse sine sweep conversion strategy -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-