AfuMathOperationOverall Enumeration¶
NXOpen.CAE.AfuMathOperation.Overall is an alias for NXOpen.CAE.AfuMathOperationOverall
-
class
NXOpen.CAE.
AfuMathOperationOverall
¶ Bases:
object
Defines the type of Overall Math Operations
Enum Members
Enum Member Enum Member Description MinimumValue Gets minimum values of AFU records MaximumValue Gets maximum values of AFU records MinimumMagnitude Gets minimum magnitude values of AFU records MaximumMagnitude Gets maximum magnitude values of AFU records MeanMagnitude Gets mean magnitude values of AFU records SumMagnitude Gets sum magnitude values of AFU records SumComplex Gets complex sum values of AFU records -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-