AfuMathOperationOutputType Enumeration¶
NXOpen.CAE.AfuMathOperation.OutputType is an alias for NXOpen.CAE.AfuMathOperationOutputType
-
class
NXOpen.CAE.
AfuMathOperationOutputType
¶ Bases:
object
Defines the output type of new AFU Data Record
Enum Members
Enum Member Enum Member Description Append Appends the new AFU Data Record to the source AFU file Overwrite Overwrites the source AFU Data Record OtherFile Saves the new AFU Data Record to other file -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-