AfuMathFastRMSInfo Class¶
-
class
NXOpen.CAE.
AfuMathFastRMSInfo
¶ Bases:
NXOpen.TransientObject
Represents the Fast RMS parameter information
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | The object destructor |
GetData | Get the Fast RMS Parameter Information |
SetData | Set the Fast RMS Parameter Information |
Method Detail¶
Dispose¶
-
AfuMathFastRMSInfo.
Dispose
¶ The object destructor
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetData¶
-
AfuMathFastRMSInfo.
GetData
¶ Get the Fast RMS Parameter Information
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (interpolationMethod, numberOfPoints, order, relativeOrder, useHighpassFilter, cutoffFraction, addSidelobes, slope) interpolationMethod is a int. the interpolation method numberOfPoints is a int. Get the Fast RMS PSD Fit number of points order is a int. the order relativeOrder is a int. the relative order useHighpassFilter is a int. the use highpass filter option cutoffFraction is a float. The filter frequency cutoff fraction addSidelobes is a int. the add sidelobes option slope is a float. the side lobes slope value New in version NX11.0.0.
License requirements: None.
SetData¶
-
AfuMathFastRMSInfo.
SetData
¶ Set the Fast RMS Parameter Information
Signature
SetData(numberOfPoints, order, relativeOrder, useHighpassFilter, cutoffFraction, addSidelobes, slope, interpolationMethod)
Parameters: - numberOfPoints (int) – Set the Fast RMS PSD Fit number of points
- order (int) – the order
- relativeOrder (int) – the relative order
- useHighpassFilter (int) – the use highpass filter option
- cutoffFraction (float) – the filter frequency cutoff fraction
- addSidelobes (int) – the add sidelobes option
- slope (float) – the side lobes slope value
- interpolationMethod (int) – the interpolation method
New in version NX11.0.0.
License requirements: None.