AfuHeaderId Class¶
-
class
NXOpen.CAE.
AfuHeaderId
¶ Bases:
NXOpen.TransientObject
the data used to create header id information for an AFU Data Record
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Coordinate | Returns or sets the coordinate of AFU Header Id |
IdLine1 | Returns or sets the id line1 of AFU Header Id |
IdLine2 | Returns or sets the id line2 of AFU Header Id |
IdLine3 | Returns or sets the id line3 of AFU Header Id |
IdLine4 | Returns or sets the id line4 of AFU Header Id |
LoadCase | Returns or sets the load case of AFU Header Id |
Owner | Returns or sets the owner of AFU Header Id |
Reference | Returns or sets the string to define reference direction sense |
ReferenceId | Returns or sets the ID of reference element or node |
Response | Returns or sets the string to define response direction sense |
ResponseId | Returns or sets the ID of response element or node |
Version | Returns or sets the version of AFU Header Id |
Property Detail¶
Coordinate¶
-
AfuHeaderId.
Coordinate
¶ Returns or sets the coordinate of AFU Header Id
-------------------------------------
Getter Method
Signature
Coordinate
Returns: the coordinate of AFU Header Id Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Coordinate
Parameters: coordinate (int) – the coordinate of AFU Header Id New in version NX5.0.0.
License requirements: None.
IdLine1¶
-
AfuHeaderId.
IdLine1
¶ Returns or sets the id line1 of AFU Header Id
-------------------------------------
Getter Method
Signature
IdLine1
Returns: the id line1 of AFU Header Id. Up to 80 characters are allowed and the redundant characters will be ignored.
Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdLine1
Parameters: idLine1 (str) – the id line1 of AFU Header Id. Up to 80 characters are allowed and the redundant characters will be ignored. New in version NX5.0.0.
License requirements: None.
IdLine2¶
-
AfuHeaderId.
IdLine2
¶ Returns or sets the id line2 of AFU Header Id
-------------------------------------
Getter Method
Signature
IdLine2
Returns: the id line2 of AFU Header Id. Up to 80 characters are allowed and the redundant characters will be ignored.
Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdLine2
Parameters: idLine2 (str) – the id line2 of AFU Header Id. Up to 80 characters are allowed and the redundant characters will be ignored. New in version NX5.0.0.
License requirements: None.
IdLine3¶
-
AfuHeaderId.
IdLine3
¶ Returns or sets the id line3 of AFU Header Id
-------------------------------------
Getter Method
Signature
IdLine3
Returns: the id line3 of AFU Header Id. Up to 80 characters are allowed and the redundant characters will be ignored.
Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdLine3
Parameters: idLine3 (str) – the id line3 of AFU Header Id. Up to 80 characters are allowed and the redundant characters will be ignored. New in version NX5.0.0.
License requirements: None.
IdLine4¶
-
AfuHeaderId.
IdLine4
¶ Returns or sets the id line4 of AFU Header Id
-------------------------------------
Getter Method
Signature
IdLine4
Returns: the id line4 of AFU Header Id. Up to 80 characters are allowed and the redundant characters will be ignored.
Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IdLine4
Parameters: idLine4 (str) – the id line4 of AFU Header Id. Up to 80 characters are allowed and the redundant characters will be ignored. New in version NX5.0.0.
License requirements: None.
LoadCase¶
-
AfuHeaderId.
LoadCase
¶ Returns or sets the load case of AFU Header Id
-------------------------------------
Getter Method
Signature
LoadCase
Returns: the load case of AFU Header Id Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadCase
Parameters: loadCase (int) – the load case of AFU Header Id New in version NX5.0.0.
License requirements: None.
Owner¶
-
AfuHeaderId.
Owner
¶ Returns or sets the owner of AFU Header Id
-------------------------------------
Getter Method
Signature
Owner
Returns: the owner of AFU Header Id. Up to 16 characters are allowed and the redundant characters will be ignored.
Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Owner
Parameters: owner (str) – the owner of AFU Header Id. Up to 16 characters are allowed and the redundant characters will be ignored. New in version NX5.0.0.
License requirements: None.
Reference¶
-
AfuHeaderId.
Reference
¶ Returns or sets the string to define reference direction sense
-------------------------------------
Getter Method
Signature
Reference
Returns: the string to define reference direction sense. Up to 4 characters are allowed and the redundant characters will be ignored. ( X, Y, Z, RX, RY, and RZ have specific meaning but the character set can be anything including a “+” or “-” as the last character. examples: ABC+ RSTU )
Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Reference
Parameters: reference (str) – the string to define reference direction sense. Up to 4 characters are allowed and the redundant characters will be ignored. ( X, Y, Z, RX, RY, and RZ have specific meaning but the character set can be anything including a “+” or “-” as the last character. examples: ABC+ RSTU ) New in version NX5.0.0.
License requirements: None.
ReferenceId¶
-
AfuHeaderId.
ReferenceId
¶ Returns or sets the ID of reference element or node
-------------------------------------
Getter Method
Signature
ReferenceId
Returns: the ID of reference element or node Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceId
Parameters: referenceId (int) – the ID of reference element or node New in version NX5.0.0.
License requirements: None.
Response¶
-
AfuHeaderId.
Response
¶ Returns or sets the string to define response direction sense
-------------------------------------
Getter Method
Signature
Response
Returns: the string to define response direction sense. Up to 4 characters are allowed and the redundant characters will be ignored. ( X, Y, Z, RX, RY, and RZ have specific meaning but the character set can be anything including a “+” or “-” as the last character. examples: ABC+ RSTU )
Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Response
Parameters: response (str) – the string to define response direction sense. Up to 4 characters are allowed and the redundant characters will be ignored. ( X, Y, Z, RX, RY, and RZ have specific meaning but the character set can be anything including a “+” or “-” as the last character. examples: ABC+ RSTU ) New in version NX5.0.0.
License requirements: None.
ResponseId¶
-
AfuHeaderId.
ResponseId
¶ Returns or sets the ID of response element or node
-------------------------------------
Getter Method
Signature
ResponseId
Returns: the ID of response element or node Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResponseId
Parameters: responseId (int) – the ID of response element or node New in version NX5.0.0.
License requirements: None.
Version¶
-
AfuHeaderId.
Version
¶ Returns or sets the version of AFU Header Id
-------------------------------------
Getter Method
Signature
Version
Returns: the version of AFU Header Id Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Version
Parameters: version (int) – the version of AFU Header Id New in version NX5.0.0.
License requirements: None.