AdaptivityMetaSolutionCollection Class

class NXOpen.CAE.AdaptivityMetaSolutionCollection

Bases: object

Represents a collection of adaptivity meta solution.

To obtain an instance of this class, refer to NXOpen.CAE.SimSimulation

New in version NX10.0.0.

Methods

Method Description
CreateBuilder Creates the builder object of adaptivity meta solution.
FindObject Finds an adaptivity meta solution with a specified name.

Method Detail

CreateBuilder

AdaptivityMetaSolutionCollection.CreateBuilder

Creates the builder object of adaptivity meta solution.

Signature CreateBuilder(metasolution)

Parameters:metasolution (NXOpen.CAE.AdaptivityMetaSolution) –
Returns:
Return type:NXOpen.CAE.AdaptivityMetaSolutionBuilder

New in version NX10.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)

FindObject

AdaptivityMetaSolutionCollection.FindObject

Finds an adaptivity meta solution with a specified name.

Signature FindObject(name)

Parameters:name (str) – name of the adpativity metasolution
Returns:The adaptivity meta solution
Return type:NXOpen.CAE.AdaptivityMetaSolution

New in version NX10.0.0.

License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)