BrushFacetsRule Class¶
-
class
NXOpen.
BrushFacetsRule
¶ Bases:
NXOpen.FacetSelectionRule
Represents a
NXOpen.FacetSelectionRule
that collects facets with brush tool intent.This rule expands to all neighboring facets of seed (and the neighbor-neighbors) that are inside brush tool. .. versionadded:: NX12.0.0
Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetData | Gets the data for the brush facets rule: NXOpen.BrushFacetsRule |
Method Detail¶
Dispose¶
-
BrushFacetsRule.
Dispose
¶ Frees the object from memory.
Signature
Dispose()
New in version NX12.0.0.
License requirements: None.
GetData¶
-
BrushFacetsRule.
GetData
¶ Gets the data for the brush facets rule:
NXOpen.BrushFacetsRule
Signature
GetData()
Returns: a tuple Return type: A tuple consisting of (brushToolStartPoint, brushToolDirection, brushToolRadius, collectInsideFacetsOnly, seedFacet) brushToolStartPoint is a
NXOpen.Point3d
. the start point of brush tool brushToolDirection is aNXOpen.Vector3d
. the vector defining direction of brush tool brushToolRadius is a float. the radius of brush tool collectInsideFacetsOnly is a bool. the flag indicating collection of inside brush facets only is allowed.seedFacet is aNXOpen.IFacet
. the seed facet .. versionadded:: NX12.0.0License requirements: gateway (“UG GATEWAY”)