OnestepUnformBuilderUnfoldMode Enumeration¶
NXOpen.BodyDes.OnestepUnformBuilder.UnfoldMode is an alias for NXOpen.BodyDes.OnestepUnformBuilderUnfoldMode
-
class
NXOpen.BodyDes.
OnestepUnformBuilderUnfoldMode
¶ Bases:
object
The Onesetp unfold mode of onestep unform.
Enum Members
Enum Member Enum Member Description Complete Onestep unfold mode is complete Intermediate Onestep unfold mode is intermediate Trimline Onestep unfold mode is trimline Unknown Onestep unfold mode is unknown -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-