OnestepUnformBuilderSurface Enumeration

NXOpen.BodyDes.OnestepUnformBuilder.Surface is an alias for NXOpen.BodyDes.OnestepUnformBuilderSurface

class NXOpen.BodyDes.OnestepUnformBuilderSurface

Bases: object

The surface types of onestep unform.

Enum Members

Enum Member Enum Member Description
Inner Onestep solver will offset inner surface and enlarge it
Middle Onestep solver will not offset middle surface
Outer Onestep solver will offset outer surface and shrink it
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.