OnestepUnformBuilderObject Enumeration

NXOpen.BodyDes.OnestepUnformBuilder.Object is an alias for NXOpen.BodyDes.OnestepUnformBuilderObject

class NXOpen.BodyDes.OnestepUnformBuilderObject

Bases: object

The object types of onestep unform.

Enum Members

Enum Member Enum Member Description
Solid solid
Face face
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.