OnestepUnformBuilderMeshElement Enumeration

NXOpen.BodyDes.OnestepUnformBuilder.MeshElement is an alias for NXOpen.BodyDes.OnestepUnformBuilderMeshElement

class NXOpen.BodyDes.OnestepUnformBuilderMeshElement

Bases: object

The 2-D mesh element type of onestep unform.

Enum Members

Enum Member Enum Member Description
Triangle Generate 2D triangle mesh element
Quadrate Generate 2D quadrate mesh element
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.