OnestepUnformBuilderDisplaySpringbackMode Enumeration

NXOpen.BodyDes.OnestepUnformBuilder.DisplaySpringbackMode is an alias for NXOpen.BodyDes.OnestepUnformBuilderDisplaySpringbackMode

class NXOpen.BodyDes.OnestepUnformBuilderDisplaySpringbackMode

Bases: object

The mode of display springback.

Enum Members

Enum Member Enum Member Description
Displacement Onestep display springback mode is displacement
Alongx Onestep display springback mode is along X
Alongy Onestep display springback mode is along Y
Alongz Onestep display springback mode is along Z
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.