OnestepUnformBuilderConstraint Enumeration

NXOpen.BodyDes.OnestepUnformBuilder.Constraint is an alias for NXOpen.BodyDes.OnestepUnformBuilderConstraint

class NXOpen.BodyDes.OnestepUnformBuilderConstraint

Bases: object

The constraints of onestep unform.

Enum Members

Enum Member Enum Member Description
CurveToCurve Curve to Curve Constraint, used for intermediate unform only
PointToPoint Point to Point Constraint, used for complete unform only
CurveAlongCurve Curve along Curve Constraint, used for complete unform only
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.