WizardTaskNavigatorItem Enumeration

NXOpen.BlockStyler.Wizard.TaskNavigatorItem is an alias for NXOpen.BlockStyler.WizardTaskNavigatorItem

class NXOpen.BlockStyler.WizardTaskNavigatorItem

Bases: object

Specifies an item in the Task Navigator.

Enum Members

Enum Member Enum Member Description
Step
SubNode
Background
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.