WizardSubNodeAction Enumeration¶
NXOpen.BlockStyler.Wizard.SubNodeAction is an alias for NXOpen.BlockStyler.WizardSubNodeAction
-
class
NXOpen.BlockStyler.
WizardSubNodeAction
¶ Bases:
object
Specifies the type of action performed on a sub-node in the Wizard Task Navigator. The action is passed into the callback BlockStyler.Wizard.OnSubNodeCallback.
Enum Members
Enum Member Enum Member Description Select Sub-node has been selected. Deselect Sub-node has been deselected. Check Sub-node has been checked if a checkbox was specified. Uncheck Sub-node has been unchecked if a checkbox was specified. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-