TreeColumnDisplay Enumeration¶
NXOpen.BlockStyler.Tree.ColumnDisplay is an alias for NXOpen.BlockStyler.TreeColumnDisplay
-
class
NXOpen.BlockStyler.
TreeColumnDisplay
¶ Bases:
object
Represents the column display type. If the type is
BlockStyler.TreeColumnDisplay.Icon
then the provided text is interpreted as icon.Enum Members
Enum Member Enum Member Description Text Text Icon Icon -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-