SelectPartFromList Class¶
-
class
NXOpen.BlockStyler.
SelectPartFromList
¶ Bases:
NXOpen.BlockStyler.UIBlock
Represents a Select Part From List block
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Enable | Returns or sets the Enable. |
Expanded | Returns or sets the Expanded |
Group | Returns or sets the Group |
Label | Returns or sets the Label |
Name | Returns the name of the block or BlockID |
Show | Returns or sets the Visibility of block. |
Tag | Returns the Tag for this object. |
Type | Returns the type of block |
Methods¶
Method | Description |
---|---|
Focus | Focuses on the block. |
GetProperties | Returns the properties of the block |
GetSelectedObjects | Gets the SelectedObjects |
SetSelectedObjects | Sets the SelectedObjects |
Method Detail¶
GetSelectedObjects¶
-
SelectPartFromList.
GetSelectedObjects
¶ Gets the SelectedObjects
Signature
GetSelectedObjects()
Returns: Value to get from the property Return type: list of NXOpen.TaggedObject
New in version NX8.5.0.
License requirements: None.
SetSelectedObjects¶
-
SelectPartFromList.
SetSelectedObjects
¶ Sets the SelectedObjects
Signature
SetSelectedObjects(objectVector)
Parameters: objectVector (list of NXOpen.TaggedObject
) – Value to set for the propertyNew in version NX8.5.0.
License requirements: None.