SelectObjectFilterType Enumeration¶
NXOpen.BlockStyler.SelectObject.FilterType is an alias for NXOpen.BlockStyler.SelectObjectFilterType
-
class
NXOpen.BlockStyler.
SelectObjectFilterType
¶ Bases:
object
Indicates the general filter type for selection.
Enum Members
Enum Member Enum Member Description Features Filter to select all feature types Faces Filter to select all face types Edges Filter to select all edge types CurvesAndEdges Filter to select all curve and edge types Components Filter to select all components SolidBodies Filter to select all solid bodies SheetBodies Filter to select all sheet bodies -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-