FolderSelection Class¶
-
class
NXOpen.BlockStyler.
FolderSelection
¶ Bases:
NXOpen.BlockStyler.UIBlock
Represents Folder Selection With Browse block
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Enable | Returns or sets the Enable. |
Expanded | Returns or sets the Expanded |
Group | Returns or sets the Group |
Label | Returns or sets the Label |
Name | Returns the name of the block or BlockID |
Path | Returns or sets the Path |
RetainStringValue | Returns or sets the RetainStringValue |
Show | Returns or sets the Visibility of block. |
Tag | Returns the Tag for this object. |
Type | Returns the type of block |
Methods¶
Method | Description |
---|---|
Focus | Focuses on the block. |
GetProperties | Returns the properties of the block |
Property Detail¶
Path¶
-
FolderSelection.
Path
¶ Returns or sets the Path
-------------------------------------
Getter Method
Signature
Path
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Path
Parameters: path (str) – New in version NX8.5.0.
License requirements: None.
RetainStringValue¶
-
FolderSelection.
RetainStringValue
¶ Returns or sets the RetainStringValue
-------------------------------------
Getter Method
Signature
RetainStringValue
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RetainStringValue
Parameters: retainStringValue (bool) – New in version NX11.0.0.
License requirements: None.