BasicEffectivityBuilder Class¶
-
class
NXOpen.
BasicEffectivityBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represent an interface class for basic effectivity block to assign or edit discrete effectivity unit values.
Also provides method to apply all units or no units effectivity.
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
EffectivityFormula | Returns the string representation of effectivity |
Tag | Returns the Tag for this object. |
UnitEffectivityValue | Returns or sets the unit effectivity value |
ValidationBasisEffectivityFormula | Returns the string representation of validation basis effectivity |
Methods¶
Method | Description |
---|---|
UpdateBuilderDetails | Update this builder with new NXOpen.CollaborativeDesign and effectivity formula |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
EffectivityFormula¶
-
BasicEffectivityBuilder.
EffectivityFormula
¶ Returns the string representation of effectivity
-------------------------------------
Getter Method
Signature
EffectivityFormula
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
UnitEffectivityValue¶
-
BasicEffectivityBuilder.
UnitEffectivityValue
¶ Returns or sets the unit effectivity value
-------------------------------------
Getter Method
Signature
UnitEffectivityValue
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UnitEffectivityValue
Parameters: unitEffectivity (int) – New in version NX8.5.0.
License requirements: None.
ValidationBasisEffectivityFormula¶
-
BasicEffectivityBuilder.
ValidationBasisEffectivityFormula
¶ Returns the string representation of validation basis effectivity
-------------------------------------
Getter Method
Signature
ValidationBasisEffectivityFormula
Returns: Return type: str New in version NX9.0.0.
License requirements: None.
Method Detail¶
UpdateBuilderDetails¶
-
BasicEffectivityBuilder.
UpdateBuilderDetails
¶ Overloaded method UpdateBuilderDetails
UpdateBuilderDetails(cd, effectivityFormulae)
UpdateBuilderDetails(cd, validationBasisFormula, effectivityFormulae)
-------------------------------------
Update this builder with new
NXOpen.CollaborativeDesign
and effectivity formulaSignature
UpdateBuilderDetails(cd, effectivityFormulae)
Parameters: - cd (
NXOpen.CollaborativeDesign
) – - effectivityFormulae (list of str) –
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Update this builder with new
NXOpen.CollaborativeDesign
, validation basis formula and effectivity formulae to edit. Effectivity formulae will be validated against provided validation basis formula.Signature
UpdateBuilderDetails(cd, validationBasisFormula, effectivityFormulae)
Parameters: - cd (
NXOpen.CollaborativeDesign
) – - validationBasisFormula (str) –
- effectivityFormulae (list of str) –
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Validate¶
-
BasicEffectivityBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.