BasePartPartPreview Enumeration¶
NXOpen.BasePart.PartPreview is an alias for NXOpen.BasePartPartPreview
-
class
NXOpen.
BasePartPartPreview
¶ Bases:
object
Specifies the preview mode of the part file.
Enum Members
Enum Member Enum Member Description NotSet No preview image is stored for the part. OnSave Create a preview image when the part is saved. OnDemand Create a preview image on demand. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-